MfgTool and USB 3.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MfgTool and USB 3.0

跳至解决方案
5,076 次查看
bdp42
Contributor IV

Hi,

I have two questions related to use the Freescale  MfgTool.

Is MfgTool 2.0 compatible with the .ini and .xml files that are used with MfgTool 1.x?

I'm currently using Mfg Tool V1.6.2.048 on Windows 7 and I know it has an issue with USB 3.0. From the following link version V1.6.2.055 fixes this issue. I can't find this on the Freescale website. Is it possible to get a pointer to this?

Thanks,

Bruno

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,573 次查看
bdp42
Contributor IV

I did manage to find this version of the MfgTool and it now works on my Windows 7 PC with USB 3.0.

Here's the link to the relevant post in case anyone else is looking for it. It's attached as a zip file - mfgtools-rel.7z.zip

https://community.freescale.com/thread/318706

Bruno

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,573 次查看
bdp42
Contributor IV

Forgot to add link I refer to in the question

https://community.freescale.com/thread/355524

Bruno

0 项奖励
回复
3,573 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Bruno

I am afraid that MfgTool 1.x and ver.2.0 are not fully compatible,

so some modification of xml/ini files may be needed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,573 次查看
bdp42
Contributor IV

Hi,

Ok, Then is it possible to get a pointer to V1.6.2.055 of the Mfg Tool. This may fix the problem I am having.

Thanks,

Bruno

0 项奖励
回复
3,574 次查看
bdp42
Contributor IV

I did manage to find this version of the MfgTool and it now works on my Windows 7 PC with USB 3.0.

Here's the link to the relevant post in case anyone else is looking for it. It's attached as a zip file - mfgtools-rel.7z.zip

https://community.freescale.com/thread/318706

Bruno

0 项奖励
回复