Memory for Android OS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory for Android OS

1,588件の閲覧回数
artemdmitriev
Contributor I

Hello!

I'd like to make a cheap custom board with Android os, based on IMX6 DUAL processor. Is it possible to boot processor from eMMC 5.0 memory? I don't understand why a many solutions use eMMC, not NAND. Is eMMC cheaper or maybe faster?  

0 件の賞賛
返信
1 返信

1,398件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Artem Dmitriev,

Yes, it is possible to boot from a eMMC 5.0, but it will run as 4.41 in terms of features so you won’t be able to use the features unique to eMMC 5.0. You can see information on how to do this on the following Community document.

https://community.nxp.com/docs/DOC-332187

There are pros and cons to using NAND or eMMC and the best option for your design may depend on cost, speed, storage capacity etc.

I hope this information helps!

Regards,

0 件の賞賛
返信