Memory density

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory density

2,766 Views
riteshpatel
Contributor II

Hi,

I am using iMX6UL in my custom board. Right now i am using 512MB DDR3L DRAM and 1GB NAND Flash.

I want to know maximum density supported for DRAM and Flash memory.

I got max density is 1GB for DDR3/3L from Table 34-1 in iMX6UL Ref Manual, Rev 0. & 2GB for LPDDR2 as there are two chip selects for LPDDR2. Please correct me if I am wrong.

I didn't found max density support for NAND and eMMC memories. Please let me know the density and reference in ref manual.

Seeking for your earliest response.

Regards,

Ritesh.

Labels (1)
0 Kudos
Reply
3 Replies

2,403 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Maximum DRAM memory size is 2GB. Please refer to Table 2-1 (System memory map)

of the i.MX6 UL Reference Manual.

As for NAND - there are no i.MX6 hardware / specified restrictions on supported size.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,403 Views
riteshpatel
Contributor II

As per Table 2-1 Max DRAM size is 2GB. That is for LPDDR2 memory.

For DDR3/3L, As per table # Table 34-1 on Page # 2049 of iMX6UL Ref manual, Max density per DDR device is 1GB, and out of Two chip selects there is only one Chip select for DDR3/3L.

That means we can interface max 1GB DDR3/3L DRAM memory. Please confirm.

0 Kudos
Reply

2,403 Views
Yuri
NXP Employee
NXP Employee

Hello,

The i.MX 6UltraLite supports single Chip Select DDR3 memory with CS0_B, ODT0, and SDCKE0.

data bus width = 16 bit ;

Column size = (up) 12 bits ;

Row size  = 16 bits ;

banks = 3 bits.

  Such parameters allow to address all available 2GB area.

Regards,

Yuri.

0 Kudos
Reply