Memory configuration for i.MX8QXP in U-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory configuration for i.MX8QXP in U-boot

4,414 Views
Maddis
Contributor IV

Hi,

I'm trying to find lpddr4 configuration for imx8qxp-mek -development board from U-boot, but either it's not there or I'm blind because I just can't seem to find it. There is one for imx8m, but that is different CPU and it's not being used. Seems that imx8qxp_mek_config - file is being used.

I see that imx8m devicetree blobs are being generated, but I haven't yet been able to find which one of them are being used (if any at u-boot). 

On i.MX6 it was easy since ddr timing was set at board-configuration file, but not so much no i.MX8 it seems.

Where I can find the lpddr4 config for i.MX8qxp-mek - board in U-boot? U-boot version seems to be u-boot-imx-2017.03.

0 Kudos
Reply
10 Replies

3,152 Views
_angelo_
Contributor III

But imx8qxp mek i have here, B0, uses 

MT53B768M32D4DT-062
LPDDR4 24G 768MX32 (3GB) 1.6 GHz

And ddr init in the scfw porting kit seems for 1.2Ghz (imx8qx_dcd_1.2GHz.cfg).

Why ?

 

 

 

0 Kudos
Reply

3,839 Views
simon_ko
Contributor III

Hi Joan.

I also want to configure LPDDR4 with i.mx8qxp.
Can I receive the setting excel file?

0 Kudos
Reply

3,839 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

3,839 Views
simon_ko
Contributor III

Hi joan.

I got the Excel configuration file from NXP Korea.

Thank you for your support.

0 Kudos
Reply

3,839 Views
joanxie
NXP TechSupport
NXP TechSupport

I will mail "i.MX8QXP Validation And MEK LPDDR4 Register Programming Aids" to you

3,839 Views
danwright
Contributor I

Hi Joan-

This might be exactly what I'm looking for too...  can you send these to me as well?  It does not appear that any code of this description is to be found for download...

Thanks!

Dan

0 Kudos
Reply

3,839 Views
joanxie
NXP TechSupport
NXP TechSupport

dwright@cumminsallison.com is this your mail address?

0 Kudos
Reply

3,839 Views
danwright
Contributor I

No- my email address is:  dan.wright@chargepoint.com.  But I have since convinced myself that the initialization of the DDR is actually in the SCU code.  And I have found this initialization in the imx-scfw-porting-kit-1.2.5 code.

0 Kudos
Reply

3,839 Views
joanxie
NXP TechSupport
NXP TechSupport

OK, since you have already figure this out , I don't send any mail to you for this question

0 Kudos
Reply

3,839 Views
Maddis
Contributor IV

Hi,

This was exactly I was looking for. Thanks!

0 Kudos
Reply