Memory Timing issue on custom board based on i.MX28

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Memory Timing issue on custom board based on i.MX28

1,987 次查看
Rt1z
Contributor I

Hi All,

We have build a custom board with i.mx280 and ddr2 from micron 64mb.Looks like its memory timing issue, we are using default bootlet setting , with obvious change , bank size to 4 banks and SDRAM_SIZE .

Issue we see : when writer to DDR2 ( DDR base to max size), its fails after some writer ( random ) , so if we add delay write and read and then write , work well.

 

So , this looks like memory timing issue. 

Will appreciate any one have experience dealing this issue , point me in right direction !!!!

Any help appreciated !!!

 

Thanks ,

 

RA  

标签 (1)
0 项奖励
回复
2 回复数

1,825 次查看
Rt1z
Contributor I

Thanks Ahmet for reply,

I did memory testing from bootlet and also from the kernel, (after linux_prep jumps to the kernel to uncompressed misc.c) 

from the boot_prep i am trying to writer all DRAM ( 64 Mbyte ) 4bytes @ a time. which fails randomly. Its pass if we adding delay (by reading back ) after each write.

same thing from the test code in the misc.c ( made sure we are writing in free mem space).

Same boot image work on my EVA board .

Any input on thing in s/w ( bootlet ) i need to change ( apart for the bank change DRAM[31] and SDRAM_SIZE) ? any help appreciated.

 

BR,

RA

0 项奖励
回复

1,825 次查看
AhmetYUCE
Contributor II
If i understand correctly you receive error messages from bootlet? If you have iMX28 EVK try running your modified bootlet on it. Although it have 8 bank memory, there shouldn't be any problem 4 bank settings. If your modified SW O.K. then do a electrical verification on DDR lines with a proper scope and active probes. Both for timing and voltage levels. There could be an issue with PCB routing, stackup or decoupling. Regards Ahmet
0 项奖励
回复