Memory Stats Issue on i.MX...? with Redboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory Stats Issue on i.MX...? with Redboot

818 Views
KrishnaPavan
Contributor II

Whenever I do a Power-On-Reset, I am getting a message like this

RAM: 0x00000000-0x1ff00000, [0x00095bf8-0x1fed1000] available
FLASH: 0x00000000 - 0x80000000, 16384 blocks of 0x00020000 bytes each.
RedBoot>

 

Issues I have..

1.RAM for i.MX51 is totally 512

So why total amount of RAM Is not used, even if there is a chance?

 

From above it can be seen that 64 MB of RAM is used and 64 MB left, why?

 

Flash:256 MB used...what is that 256 MB? [ 256 MB =16384 blocks of 16 KB each]

 

What can you infer from these stats......?                 Regards:: Krishna Pavan

Labels (1)
Tags (2)
0 Kudos
Reply
0 Replies