Measurements with coremark on the IMX8QXP MEK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Measurements with coremark on the IMX8QXP MEK

2,434 Views
teo1
Contributor I

Hello,

I'm working on the IMX8QXP MEK and I would like to take some consumption measures on this card.

I think that the document "i.MX 8QuadXPlus Power and Performance" is really helpfull but there are some points I don't get.

First, I would like to know how can I put the card in each KS (Key State mode), do I have to shut down the components manually or is there a program that can put the card in the KS I want automatically?
My second issue is to understand how I can use Coremark on this board. I have installed IAR IDE and downloaded coremark-main file but I can't reach to use it to take some measures.

Could someone help me please?
Thanks a lot for your help,

Best regards,
Teo

Tags (1)
0 Kudos
Reply
5 Replies

2,422 Views
igorpadykov
NXP Employee
NXP Employee

Hi Teo

 

for using coremark (sorry for m4 such documentation is not available) one can try to follow

sect.4.2.1. CoreMark only, sect.8.2.2. Steps – Coremark/Dhrystone/Stream/WhetstoneSP

AN12338  i.MX 8QuadXPlus Power Consumption Measurement

For M4 one can try to adapt CoreMark library to SDK using AN12284

https://www.nxp.com/doc/AN12284

 

Best regards
igor

0 Kudos
Reply

2,414 Views
teo1
Contributor I

Hello Igor,

Thank you for your fast answer.

I already tried to use the documents you suggested me, but when I try to run the code in the sect 8.2.2 in "Power consumption Measurement" document, I get the following answer when I run the line : echo 1 > /sys/class/graphics/fb0/blank; : "No such file or directory".

Furthermore could you explain me what you mean by "adapt Coremark library to SDK"?

Best regards,
Teo

0 Kudos
Reply

2,406 Views
igorpadykov
NXP Employee
NXP Employee

> what you mean by "adapt Coremark library to SDK"?

 

port this library to M4 SDK_MEK-MIMX8QX using sect.2.1 Porting CoreMark library AN12284

it mentions IAR Workbench IDE.

 

Best regards
igor

0 Kudos
Reply

2,402 Views
teo1
Contributor I

I don't find any project  as the lpc5500_coremark_iar\coremark.eww one which is mentionned in the document. That is why I am blocked at this point.

I thought I would fin a project in the coremark_main file but I can't find any project to load on IAR.

Best regards,
Teo

0 Kudos
Reply

2,400 Views
igorpadykov
NXP Employee
NXP Employee

suggest to post it to lpc community:

https://community.nxp.com/t5/LPC-Microcontrollers/bd-p/lpc

 

Best regards
igor

 

0 Kudos
Reply