Max speed of SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Max speed of SPI

2,027 次查看
nagamaheshg
Contributor III

We are testing SPI interface using spidev on i.MX6dl, need to check the max speed of SPI which I have set to 50Mhz in dst files.

When we set the max clock speed in our program above 30Mhz there is no effect on the clock speed, it is capped @30Mhz.

Is this a limitation ?

标签 (1)
0 项奖励
回复
1 回复

1,369 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nagamahesh

please check ecspi max. speed in Table 48. ECSPI Master Mode Timing Parameters

i.MX6SDL Datasheet
http://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复