Max clock source for PIT on iMX RT1010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max clock source for PIT on iMX RT1010

917 Views
youngSheldon
Contributor III

What is the max clock freq I can use and how to do that when using a PIT in iMXRT1010?

Datasheet mentions 100MHZ, but the clock tool in MCUXpresso specifies max freq to be 75MHz as seen below. This is a bit frustrating since PIT chapter in the latest datasheet doesn't even mention how to select the clock source for it (luckily the IDE can do it). It is probably hidden in the CCM but still frustrating as I need to read a full datasheet to configure a pheripheral instead of having at least all the references (with page numbers) in one place.

youngSheldon_0-1702899747589.png

 

 

youngSheldon_1-1702899803761.png

 

let it flow
0 Kudos
Reply
1 Reply

867 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

I apologize for the confusion the documentation might bring let me report it so it can be corrected. The maximum clock for these peripherals is limited to 75 MHz.

Best regards,
Omar

0 Kudos
Reply