Manufacturing tool for iMX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Manufacturing tool for iMX

3,544件の閲覧回数
mathew_k_t
Contributor II

Hi,

I wanna flash my emmc using manufacturing tool. But i found following difficulties in the manufacturing tool

  1. The downloaded file contains two directories with rootfs and without rootfs. Which I have to choose?
  2. How to install manufacturing tool, whether it requires any drivers?
  3. How to program emmc using Mfg tool?

Thanks

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,997件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello

The difference in the Manufacturing tool with rootfs and without rootfs, I explained you in your other community question.

Manufacturing tool for iMX 

Manufacturing tool doesn't need to be installed, is an executable file. You only need to run the script, but take note that you need to have the image in the correct folder. Otherwise, the script won't work.

To program the emmc, you only need to run the correct script that allows you to program the emmc.

Best Regards,

Diego.

0 件の賞賛
返信

2,997件の閲覧回数
mathew_k_t
Contributor II

Hi,

My mfg tool giving following error

can't find PMIC:PFUZE100

how to solve this.?

Also the default images in the mfgtool seems different from the images that I created(difference in name).

mfgtool error.png

0 件の賞賛
返信

2,997件の閲覧回数
mathew_k_t
Contributor II

Thanks Diego,

What will be the boot setting(SW601,SW602) for iMX6ULL evk while

implementing manufacturing tool

On Wed, Jan 24, 2018 at 6:15 AM, diegoadrian <[email protected]>

0 件の賞賛
返信