Manufacturing tool for iMX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Manufacturing tool for iMX

1,897 Views
mathew_k_t
Contributor II

Hi,

I downloaded MfgTool for iMX. But it contains two directories, with rootfs and without rootfs. Since i'm new to this could someone help me to install and guide me how to use it?

I'm using iMX6ULL evk. Version 4.1.15

Labels (3)
0 Kudos
Reply
1 Reply

1,589 Views
diegoadrian
NXP Employee
NXP Employee

Hello

The difference of the Manufacturing Tool with rootfs and without rootfs. Is that the Manufacturing Tool without rootfs, doesn't include a prebuild image and the Manufacturing tool with rootfs includes a minimal prebuild image. However, I recommend you to use the Manufacturing tool with rootfs, because you can know where you need to place the Yocto image that you created, giving the case that you are using your own Yocto image.

Furthermore, if you are interested in the Yocto project and you are willing to learn more about it. I highly recommend you to visit the below training:

Yocto Training - home 

Best Regards,

Diego.

0 Kudos
Reply