Mainstream kernel support for imx6ul

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mainstream kernel support for imx6ul

1,716件の閲覧回数
feae
Contributor I

Hello,

I'm working in a project that will support Linux in imx6ul and atmel boards. So, I'd like to know what is the status of the imx6ul support in the mainstream kernels 4.x.

Thanks for your help,

Fernando A. E.

ラベル(2)
0 件の賞賛
返信
1 返信

1,505件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Fernando A. E.,

There are a couple of BSP Releases for NXP’s boards based on kernel 4.X. You can see them on the following link:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

There is also a Community BSP which is part of the Yocto Project and maintained by the community and this supports also 3rd party boards and kernel revisions different than the BSP Releases which are somewhat limited.

http://freescale.github.io/

I would recommend looking for these kernels when working on the i.MX6UL as porting a kernel from mainline may be time consuming.

Regards,

0 件の賞賛
返信