Mainstream kernel support for imx6ul

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mainstream kernel support for imx6ul

1,715 Views
feae
Contributor I

Hello,

I'm working in a project that will support Linux in imx6ul and atmel boards. So, I'd like to know what is the status of the imx6ul support in the mainstream kernels 4.x.

Thanks for your help,

Fernando A. E.

Labels (2)
0 Kudos
Reply
1 Reply

1,504 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Fernando A. E.,

There are a couple of BSP Releases for NXP’s boards based on kernel 4.X. You can see them on the following link:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

There is also a Community BSP which is part of the Yocto Project and maintained by the community and this supports also 3rd party boards and kernel revisions different than the BSP Releases which are somewhat limited.

http://freescale.github.io/

I would recommend looking for these kernels when working on the i.MX6UL as porting a kernel from mainline may be time consuming.

Regards,

0 Kudos
Reply