.MX8MP doesn't support virtual channels.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

.MX8MP doesn't support virtual channels.

605 Views
nesnes
Contributor I

 

We're currently working on an application where we need to use multiple cameras and stream from them simultaneously. We're planning to use FDP Link or GMSL cameras for this. However, we've noticed that the i.MX8MP doesn't support virtual channels.

I have a couple of questions:

  1. What are the limitations with the i.MX8MP in this context?
  2. Is there another MPU recommended by NXP that could handle this better?

We already have a product using the i.MX8MP, so any suggestions would be really helpful. If you could provide specific feedback regarding the i.MX8MP, that would be great.

0 Kudos
Reply
3 Replies

517 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @nesnes

Thank you for contacting NXP Support!

1. What are the limitations with the i.MX8MP in this context?

As you mentioned, I can confirm that i.MX8MP doesn't support virtual channels.
The i.MX8MP can supports up to 2 cameras with MIPI-CSI interface.

2. Is there another MPU recommended by NXP that could handle this better?

Regarding, our MPU product family i.MX8 you can use the i.MX8Quad Max that supports multiple cameras.
Please have a look to the following reference to support multiple cameras:

Working With Multiple Cameras in i.MX8 - NXP Community

0 Kudos
Reply

567 Views
nesnes
Contributor I

I’m waiting for your answers and suggestions about i.MX8MP. 

0 Kudos
Reply

539 Views
davidty
Contributor I

I'm also waiting for instructions. I also had the same problem as you. I think they have a solution

Community Camera Viet Nam: Thu mua camera
0 Kudos
Reply