MX8M-MINI RPA_v14

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8M-MINI RPA_v14

5,781 Views
aviad_h
Senior Contributor I

Hi,

Referring to the latest RPA " MX8M_Mini_DDR4_RPA_v14.xlsx" posted by NXP

According to revision table the CL setting (F28) for MT40A512M16LY-075:E has been updated to be in line with the datasheet and set to 17.

However in the datasheet of Micron P/N: MT40A512M16LY-075:E Table 1 for 075:E speed grade the CL value is 18 

Can you please explain the reason for the difference?

I wish to use Samsung P/N: K4A8G165WC-BCTD

it seems from datasheet Table 2 that CL=19 but this value is not an option in F28 drop down menu

Thank you for your support,

Aviad

0 Kudos
Reply
8 Replies

5,721 Views
aviad_h
Senior Contributor I

Hi,

Referring to Micron device, can you please explain your deduction of CL=17, is it according to speed grade -083 "READ CL: non-DBI"?

For that matter, why is that preferred over -083E, -083D corresponding values 16/18?

Thank you,

Aviad

0 Kudos
Reply

5,752 Views
Yuri
NXP Employee
NXP Employee

@aviad_h 
Hello,

   The Excel table (aid tool) comments parameter READ Latency (CL)
as following: "Please refer to the speed bin tables in the device
data sheet for CL settings that are supported for the chosen data
rate/clock cycle."

  The CL = 17 is taken from Table 158(DDR4-2400 Speed Bins and
Operating Conditions) of the memory Datasheet. Note: value CL=18
also is possible and may be considered as more "safe".

Regards,
Yuri.

0 Kudos
Reply

5,742 Views
aviad_h
Senior Contributor I

Hi,

The -075E ending of Micron P/N implies that speed grade is DDR4-2666 (See Table 1)

To my understanding "Table 159: DDR4-2666" is the corresponding table.1.png

Therefore my question is

1. Which is correct value for NXP Micron P/N: MT40A512M16LY-075:E

2. Which is correct value for Samsung P/N:  K4A8G165WC-BCTD ? Would 18 which is the max value in RPA tool be OK?

Thank you for your support,

Aviad

0 Kudos
Reply

5,731 Views
Yuri
NXP Employee
NXP Employee

@aviad_h 
Hello,

   1) It makes sense to use  timing parameters for the working memory frequency (DDR4-2400),
       but not for max  frequency (DDR4-2666).
  2) As for the Samsung device - please consult with them for assurance.

  

Regards,
Yuri.

0 Kudos
Reply

5,714 Views
aviad_h
Senior Contributor I

Hi,

Referring to Micron device, can you please explain your deduction of CL=17, is it according to speed grade -083 "READ CL: non-DBI"?

For that matter, why is that preferred over -083E, -083D corresponding values 16/18?

Thank you,

Aviad

0 Kudos
Reply

5,707 Views
Yuri
NXP Employee
NXP Employee

@aviad_h 
Hello,

   CL=17 configuration was tested.

Regards,
Yuri.

0 Kudos
Reply

5,702 Views
aviad_h
Senior Contributor I

Hi,

I apologize but the answer is not clear.

Can you please explain based on table 158 how this value was chosen, what cell in specific and why? if the value was selected arbitrarily and just tested please notify as well. This is required in order to be able to select correctly value for Samsung device.

Thank you for your support

Aviad

0 Kudos
Reply

5,700 Views
Yuri
NXP Employee
NXP Employee

@aviad_h 

   You may select more "safe" value CL=18 (comparing with 17) and check it,
using the Stress memory test. If all is OK and there is - at least theoretical -
option CL=17 - why do not try and test it.
 

~Yuri.

0 Kudos
Reply