MX6UL UART2 RXProblem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MX6UL UART2 RXProblem

2,962 次查看
nachodiz
Contributor III

Dear all

UART2 from our custom MX6UL board is attached to a RN4871 Bluetooth Module

UART2 TX works fine but RX is not working

How can i configure uart2 rx properly?


UART2.png

King Regards

标签 (5)
0 项奖励
回复
4 回复数

2,552 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 Please read the dtb (as is, in binary) from the board and send me. 

Regards,

Yuri.

0 项奖励
回复

2,552 次查看
Yuri
NXP Employee
NXP Employee

Hello, nachodiz !

  from Your dtb configuration for UART2 :

serial@021e8000 {
compatible = "fsl,imx6ul-uart", "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x21e8000 0x4000>;
interrupts = <0x0 0x1b 0x4>;
clocks = <0x1 0xbf 0x1 0xc0>;
clock-names = "ipg", "per";
dmas = <0x7 0x1b 0x4 0x0 0x7 0x1c 0x4 0x0>;
dma-names = "rx", "tx";
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <0x37>;
fsl,uart-has-rtscts;
};

  First - RTS/CTS is not used on Your scheme, therefore  line "fsl,uart-has-rtscts;"

should be removed. Further - DMA cannot be used without RTS/CTS, so lines "dmas"

and "dma-names"  should be removed too. You may try enclosed dtb file.

  Note - high speeds cannot be used without DMA.

Regards,

Yuri.

0 项奖励
回复

2,552 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please check (and modify if needed) under Linux :
1) IOMUXC_SW_MUX_CTL_PAD_UART2_RX_DATA register (0x20E_0098) :
     if  bit field mux_mode = 0.
2) IOMUXC_UART2_RX_DATA_SELECT_INPUT ( 0x20E_062C) :
  if bit field DAISY = 01.

You may use memtool utility, located in /unit_tests directory of NXP BSP.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,552 次查看
stevenyu
Contributor III

Dear Yuri,

Recently, we use i.mx6ull and try to enable UART5, and then initialize it to be RS-232. 

We can have TX working by echo "hello" > /dev/ttymxc4, and the "hello" will be show on PC console.

However, the RX path from PC console to i.mx6ull does not work.

We want to try the comment you mentioned. Would you please advise where can we configure these two parameters ?

IOMUXC_SW_MUX_CTL_PAD_UART2_RX_DATA / IOMUXC_UART2_RX_DATA_SELECT_INPUT

1) IOMUXC_SW_MUX_CTL_PAD_UART2_RX_DATA register (0x20E_0098) : 
     if  bit field mux_mode = 0.
2) IOMUXC_UART2_RX_DATA_SELECT_INPUT ( 0x20E_062C) :
  if bit field DAISY = 01.

Do you have any experience to configure UART on i.mx6ul to be RS-232/RS-485 ?

 

Regards,

Steven Yu

0 项奖励
回复