MX6UL_SNVS_LP and POR pull-up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX6UL_SNVS_LP and POR pull-up

1,357件の閲覧回数
sguy
Contributor III

Hi,

I saw on the u-boot code that the POR_B pull-up can be configured using the register on (MX6UL_SNVS_LP_BASE_ADDR + 0x10).

I couldn't find the documentation of this register on the IMX6URM (Rev. 1) and not on the IMX6ULSRM (Rev. C).

Where is this register documented?

ラベル(1)
0 件の賞賛
返信
1 返信

1,177件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

which register do you need? SNVS_LP is low power doman, if you couldn't find the register from Reference Manual, one can refer to the source code, in fact some internal registers, customer don't need to change it.

0 件の賞賛
返信