MX6UL_SNVS_LP and POR pull-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX6UL_SNVS_LP and POR pull-up

629 Views
sguy
Contributor III

Hi,

I saw on the u-boot code that the POR_B pull-up can be configured using the register on (MX6UL_SNVS_LP_BASE_ADDR + 0x10).

I couldn't find the documentation of this register on the IMX6URM (Rev. 1) and not on the IMX6ULSRM (Rev. C).

Where is this register documented?

Labels (1)
0 Kudos
Reply
1 Reply

449 Views
joanxie
NXP TechSupport
NXP TechSupport

which register do you need? SNVS_LP is low power doman, if you couldn't find the register from Reference Manual, one can refer to the source code, in fact some internal registers, customer don't need to change it.

0 Kudos
Reply