MX6 encoding SXGA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX6 encoding SXGA

1,550 Views
timothybean
Contributor IV

Could someone tell me if encoding an SXGA via CSI port is possible at 60 fps? I saw another post that indicated that it would not be possible at that frame rate, but running the VPU at 266 MHZ. What about running it at 350 MHZ? Could it be possible then to encode that resolution at 60 fps?

Thanks

Tim

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,453 Views
joanxie
NXP TechSupport
NXP TechSupport

it depends what data format you use, if the number of cycles needed to send a single pixel is one, yes mx6 IPU can support it, for more detailed information, you can refer to the chapter 37.1.2.1.1 Camera Ports of Reference Manual, the formula is:

F = FH * FW * FPS * BI * DF

0 Kudos
Reply