MX6 encoding SXGA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX6 encoding SXGA

1,548件の閲覧回数
timothybean
Contributor IV

Could someone tell me if encoding an SXGA via CSI port is possible at 60 fps? I saw another post that indicated that it would not be possible at that frame rate, but running the VPU at 266 MHZ. What about running it at 350 MHZ? Could it be possible then to encode that resolution at 60 fps?

Thanks

Tim

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,451件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

it depends what data format you use, if the number of cycles needed to send a single pixel is one, yes mx6 IPU can support it, for more detailed information, you can refer to the chapter 37.1.2.1.1 Camera Ports of Reference Manual, the formula is:

F = FH * FW * FPS * BI * DF

0 件の賞賛
返信