MX53 Linux platform successfully launch, Yuanying Tech.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX53 Linux platform successfully launch, Yuanying Tech.

6,159 Views
Oceanblue
Contributor III

        As one technical leading company, in past few year Yuanying Tech always focus on embedded system solution offering, from low end to high end. Our platform including MX25, MX28, MX35 and MX51. From Nov of last year, Yuanying Tech. have started to design MX53 platform based on Linux OS. Now, we have successfully finished this project and launched MX53 Linux OS embedded system platform --- YY- i.MX53L。

 

         i.MX53L is an Linux System Platform based on Linux-2.6.35 kernel, adopt ext2 file system, designed by Yuan-ying Technology. i.MX53L own plentiful peripheral interface, such as USB HOST, USB OTG, TVE Output、DVI、VGA、LVDS、Camera CSI input、SDIO and so on, i.MX53L is widely applied various field, including: HD internet monitor/Automotive Infotainment, industrial computer and thin client machine(cloud computer), MID , Home Media Terminal, V2IP, Factory Automation, HMI design, etc. The dual display feature is the most suitable platform for education equipment. Customer need only focus on the application software design, and largely shorten the time to market cycle.

Labels (1)
0 Kudos
Reply
3 Replies

6,035 Views
KrishnaPavan
Contributor II
Can you provide me the System Boot Flow, the Relevant programs associated with and the concept of NAND Boot flow?
0 Kudos
Reply

6,035 Views
richard0909
Contributor I
Does it support Android?
0 Kudos
Reply

6,035 Views
Oceanblue
Contributor III

690-IMG_0008.jpg

 

         MX53 system board overview from Yuanying Tech.

         Visiting www.yuan-ying.com for the detail. meanwhile, Yuanying Tech. support the mini system board selling alone to speed up customer project design.

0 Kudos
Reply