MX51 Linux Platform for Embedded application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX51 Linux Platform for Embedded application

1,278件の閲覧回数
Oceanblue
Contributor III

     From 2009, Yuan-ying Technology invest to design MX51 platform, by now we have successfully launched i.MX25 and i.MX35 development platform and the related turn key solution. To meet the market demand and the end user request, Yuan-ying Technology has launched MX51 Linux OS development platform --- YY-MX51L。

       

      YY-MX51L is an Linux Platform system based on Linux-2.6.31 kernel, consist of core module and base board ,and adopt ext2 file system, designed by Yuan-ying Technology. i.MX51L own plateful peripheral interface, such as USB HOST, USB OTG, TVE Output、DVI、VGA、LVDS、TFT LCD、SDIO and so on, i.MX5L is widely applied various field, including:  Consumer Electronic/Automotive Infotainment, industrial computer and industrial control. Which is the most suitable platform for tablet/Smart Book, Smartphone, MID, E-book, Digital Picture Frame, Home Media Terminal, V2IP, Car Multimedia, Industrial Computer, Factory Automation, HMI design.

       Yuanying Tech. support core module selling model, end customers only focus on software development and based board re-layout, largely shorten product design cycle. Visiting www.yuan-ying.com for more details.

        595-Linux_LCD.jpg

0 件の賞賛
返信
0 返答(返信)