MX28 WinCE6 USB enumeration issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MX28 WinCE6 USB enumeration issue

1,491 次查看
Rodrigue
NXP Employee
NXP Employee

Dear Support,

Customer have a device that is not enumerating properly on the TX28 from Karo (SOM manufacturer) units with Windows CE 6.0.  It contains an interface that lists zero as the number of endpoints.  As far I know, this is a valid interface that uses only the control endpoint.

However, the enumeration fails when determining the number of interfaces.

Specifically, in BSP/common/src/soc/COMMON_FSL_V3/MS/USBH/USB2COM/cdevice.cpp, the CreateUsbConfigurationStructure() call fails in the "second step". 

The buffer contains 18 bytes, which correspond to a configuration descriptor and an interface descriptor.  The interface descriptor specifies bNumEndpoints == 0, and there are also no additional interfaces.  Therefore, 18 is the complete length of the data for the two descriptors.

The code has a test:

while (offset + x + sizeof(USB_INTERFACE_DESCRIPTOR) < dataBufferLen)

where offset=9, x=0, and dataBufferLen=18.

Therefore, the test fails, preventing the number of interfaces from being incremented, and resulting in a failure of the entire enumeration.

Changing the '<' to '<=' seems to resolve the problem.

Can we confirm this is an issue?

It seems that both WinCE 6.0 & WinCE 7.0 use the same conditional statement, so presumably both will fail, but only WinCE6 was tested.

Br,

Rod

0 项奖励
回复
1 回复

1,183 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Deactivated user can you help on this case?

0 项奖励
回复