MX25 Linux Embedded platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MX25 Linux Embedded platform

958 次查看
Oceanblue
Contributor III

      Starting from Oct,2009 , YUANYING Tech has invested a lot of resource in the system design with FREESCALE ARM series product, up to date we have launched the series development platform based on i.MX28、i.MX35、i.MX51,largely help our customers shorten the time to market about their product and create the success one and another. Now we are proud to announce we have launched i.MX25 Linux system level platform:YY-MX25L。

      

       YY-X25L is the system platform based on Linux 2.6.31 kernel,treat ext2 as system file,  own i.mx258+128MB DDR2 system hardware, be able to boot up form SD card or NAND Flash,also i.MX25L including 7” LCD and resistance touch panel. Which built in i.MX25 all input/output resource. Which still adopt core board + bottom board structure,the components of CPU core board meet the industrial level,be able to work at the temperature range of -40C to +85C,and storage temperature from  -55C to +125 degree. i.MX25L can widely applied for intelligent electric network, outdoor multimedia, industrial control and HMI, medical equipment and so on .Which is the good selection to power meter terminal, HMI of industry equipment, automotive ECU, medical device display interface。

       

      About the business model, YUANYING support core board selling and PCBA business model. And, promise to deliver the cost effective performance among ARM9 system to her customers.Visiting www.yuan-ying.com for more details.

591-MX25Linux_LCD.jpg

0 项奖励
回复
0 回复数