MT9V032 camera on parallel port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MT9V032 camera on parallel port

1,698 Views
richardwoodham
Contributor I

Linux version 4.1.15

Machine model: Variscite i.MX6 QUAD VAR-DART Smart Device Board

I added mt9v032 support using menuconfig & added an entry (marked here in bold)

&i2c3 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c3_3>;
status = "okay";

/* DS1307 RTC module */
rtc@0x68 {
compatible = "dallas,ds1307";
reg = <0x68>;
};

mt9v032@5c {
compatible = "aptina,mt9v032";
reg = <0x5c>;

port {
mt9v032_out: endpoint {
link-frequencies = /bits/ 64
<13000000 26600000 27000000>;
};
};
};
};

to the .dtsi file.  On boot I get:

[ 1.440565] mt9v032: probe of 2-005c failed with error -2

What does this message mean?  The I2C hardware works.  I can use i2cdetect to prove it - 0x56 is detected & I can see it on the scope (response is 0x13 - check it out in the datasheet).

The scope says that 0x5c is not being probed during boot (0x68 is).  Why not?

Labels (4)
Tags (2)
0 Kudos
Reply
1 Reply

1,471 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

one can try to debug it in probe function with oscilloscope

[RFC,media] mt9v032: Add support for mt9v022 and mt9v024 - Patchwork 

using AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf

also seems phytec has support for this sensor:

ftp://ftp.phytec.de/pub/ImageProcessing/phyFLEX-i.MX6_linux_PD15.1.1/Software/Camera_Patch_PD15.1.1/...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply