MT53E1G32D2FW-046 WT:B || LPDDR with IMX8M PLUS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MT53E1G32D2FW-046 WT:B || LPDDR with IMX8M PLUS

821 Views
JyotiVaishnav
Contributor II

Hi NXP Team, 

We are using  IMX8M Plus  and are planning to use the following LPDDR. Could you please look into this and confirm that the suggested part can be used.
 
Processor : MIMX8ML6CVNKZAB
LPDDR : MT53E1G32D2FW-046 WT:B
 
The Software details are mentioned below, anything need to be taken card from software side when changing the LPDDR from 6GB to 4GB.  
Yocto 4.2_mickledore
kernel version 6.1.36
U boot version v2023.04
 
Please refer to the LPDDR Datasheet below 
0 Kudos
Reply
2 Replies

301 Views
rcossdev
Contributor I

Hello JyotiVaishnav,

Did you manage to generate the lpddr4_timing.c file?

We designed a board based also on the imx8mp using the same RAM (MT53E1G32D2FW)
But since we didn't include the OTG circuitry we're unable to run the ddr tool and we're struggling to do the bring-up of the board.

I'd really appreciate if you could share your timing file.

Regards!

0 Kudos
Reply

799 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply