MSI Interrupt Message Address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSI Interrupt Message Address

2,772 Views
iqrajaved
Contributor III

Hi, 

I am working on implementation of PCIe driver for IMX6 platform. The basic functionality of driver is working fine and tested. But in case of MSI, i am a bit confused that what should be the value written to MSI message address register in the MSI capabilities register set of EP? I didn't find anything clearly written in the Technical Reference Manual. All it says is that the address should be common in MSI capabilities as well as MSI controller address register. The screenshot is also added for this. 

pastedImage_1.png

Can anyone please guide me about this? May be there is something that I am overlooking.

Thank you in anticipation.

Iqra Javed

2 Replies

2,569 Views
iqrajaved
Contributor III

Thank you b45499‌ for replying. 

I did try that thread. But its not clearly mentioned there too what should be written in the MSI Address Regiter of Capabilities of Endpoint and MSI controller address register. 

0 Kudos
Reply

2,569 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can try to refer to the thread in our community https://community.nxp.com/thread/464959. Hope this can do help for you.

Have a nice day

Rita