MSCALE-SECO FW version issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSCALE-SECO FW version issue

Jump to solution
1,892 Views
PBR
Contributor IV

Hi,

 

I have to check the DDR4 of my new custom board with a IMX8QXP-C0.

I am using MSCALE software: mx8_ddr_stress_test_ER14_installation.zip which seems the latest.

This one is working on my IMX8QXP EVM board but not on my custom board.

The IMX8QXP-C0 on my board has no installed firmware and is configured in serial boot mode.

Please see me attached log files: one with my EVM board and one with my custom board. There are really different. Why?

On the custom board (DDR-UBR.log), it is written at the end:

"Incorrect SECO FW version 2.5.4 (2.6.0 or later required)"

The Seco FW is given by the Mscale, am I right? So does it mean my Mscale is not the latest? Do you have a new one?

Or do I need to download a Seco FW prior using Mscale? With uuu?

 

Thank you for your help.

0 Kudos
Reply
1 Solution
1,871 Views
PBR
Contributor IV

I discovered the problem, I was on the wrong UART (I was on SCU UART, not UART0).

Note: even with a new board without SCFW or any software, the DDR tools is working correctly.

 

View solution in original post

0 Kudos
Reply
2 Replies
1,872 Views
PBR
Contributor IV

I discovered the problem, I was on the wrong UART (I was on SCU UART, not UART0).

Note: even with a new board without SCFW or any software, the DDR tools is working correctly.

 

0 Kudos
Reply
1,880 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply