MQS example schematic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQS example schematic

3,276件の閲覧回数
cbrake
Contributor III

Are there an example schematics for i.MX6UL MQS (Medium quality sound)?  Is this really as simple as connecting the output directly to an audio amp?

Also, is there a linux driver available for MQS?

Thanks,
Cliff

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,265件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The i.MX6UL  MQS is used to generate medium quality audio via standard GPIO
and produces PWM signal, fixed in amplitude and frequence, but varying in
duty cycle. So additional RC filter is needed at output, this will produce
medium quality sound without an additional DAC.

Regards,

Yuri.

0 件の賞賛
返信

2,265件の閲覧回数
b36401
NXP Employee
NXP Employee

No. We have no such schematic example.

You are supposed to create a schematic yourself.

Sorry for the inconvenience.

i.MX6UL processor have such interface: MQS_LEFT and MQS_RIGHT pins.

They are PWM encoded. So you can connect audio amplifier to them with a filter.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信