MQS example schematic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQS example schematic

3,280 Views
cbrake
Contributor III

Are there an example schematics for i.MX6UL MQS (Medium quality sound)?  Is this really as simple as connecting the output directly to an audio amp?

Also, is there a linux driver available for MQS?

Thanks,
Cliff

Labels (2)
0 Kudos
Reply
2 Replies

2,269 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The i.MX6UL  MQS is used to generate medium quality audio via standard GPIO
and produces PWM signal, fixed in amplitude and frequence, but varying in
duty cycle. So additional RC filter is needed at output, this will produce
medium quality sound without an additional DAC.

Regards,

Yuri.

0 Kudos
Reply

2,269 Views
b36401
NXP Employee
NXP Employee

No. We have no such schematic example.

You are supposed to create a schematic yourself.

Sorry for the inconvenience.

i.MX6UL processor have such interface: MQS_LEFT and MQS_RIGHT pins.

They are PWM encoded. So you can connect audio amplifier to them with a filter.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply