MPlayer Configuration Options

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPlayer Configuration Options

跳至解决方案
2,065 次查看
erickang
Contributor II

Dear all,

I have a problem to display the video file in the i.MX25.

 

I'm using the MPlayer to display the video file.

But the dispaly speed is slow.

 

So I checked the MPlayer profile for the source Video file.

In the profile, I had been found the YUV to RGB conversion had much load in the MPlayer.

The simple profile contents are like below. For the detailed, refer to the attach file. (mplayer_profile_1.txt)

 

I think I could reduce the load of YUV2RGB function if I optimize the MPlayer to the i.MX25 core.

The i.MX257 core is ARM9, and the model number is "ARM926EJ-S".

 

Could you tell me the MPlayer Configuration options for i.MX257 ARM Core?

 

Best Regards,

Eric.

Original Attachment has been moved to: mplayer_profile_1.txt.zip

标签 (3)
标记 (3)
0 项奖励
回复
1 解答
1,635 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX25, there is no IPU and VPU, video decoding only can do it in software way so the performance is not good.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,636 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX25, there is no IPU and VPU, video decoding only can do it in software way so the performance is not good.

0 项奖励
回复
1,635 次查看
erickang
Contributor II

Thanks jimmychan,

0 项奖励
回复