MPlayer Configuration Options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPlayer Configuration Options

Jump to solution
3,047 Views
erickang
Contributor II

Dear all,

I have a problem to display the video file in the i.MX25.

 

I'm using the MPlayer to display the video file.

But the dispaly speed is slow.

 

So I checked the MPlayer profile for the source Video file.

In the profile, I had been found the YUV to RGB conversion had much load in the MPlayer.

The simple profile contents are like below. For the detailed, refer to the attach file. (mplayer_profile_1.txt)

 

I think I could reduce the load of YUV2RGB function if I optimize the MPlayer to the i.MX25 core.

The i.MX257 core is ARM9, and the model number is "ARM926EJ-S".

 

Could you tell me the MPlayer Configuration options for i.MX257 ARM Core?

 

Best Regards,

Eric.

Original Attachment has been moved to: mplayer_profile_1.txt.zip

Labels (3)
0 Kudos
Reply
1 Solution
2,617 Views
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX25, there is no IPU and VPU, video decoding only can do it in software way so the performance is not good.

View solution in original post

0 Kudos
Reply
2 Replies
2,618 Views
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX25, there is no IPU and VPU, video decoding only can do it in software way so the performance is not good.

0 Kudos
Reply
2,617 Views
erickang
Contributor II

Thanks jimmychan,

0 Kudos
Reply