MPlayer Configuration Options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPlayer Configuration Options

ソリューションへジャンプ
3,044件の閲覧回数
erickang
Contributor II

Dear all,

I have a problem to display the video file in the i.MX25.

 

I'm using the MPlayer to display the video file.

But the dispaly speed is slow.

 

So I checked the MPlayer profile for the source Video file.

In the profile, I had been found the YUV to RGB conversion had much load in the MPlayer.

The simple profile contents are like below. For the detailed, refer to the attach file. (mplayer_profile_1.txt)

 

I think I could reduce the load of YUV2RGB function if I optimize the MPlayer to the i.MX25 core.

The i.MX257 core is ARM9, and the model number is "ARM926EJ-S".

 

Could you tell me the MPlayer Configuration options for i.MX257 ARM Core?

 

Best Regards,

Eric.

Original Attachment has been moved to: mplayer_profile_1.txt.zip

ラベル(3)
0 件の賞賛
返信
1 解決策
2,614件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX25, there is no IPU and VPU, video decoding only can do it in software way so the performance is not good.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,615件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX25, there is no IPU and VPU, video decoding only can do it in software way so the performance is not good.

0 件の賞賛
返信
2,614件の閲覧回数
erickang
Contributor II

Thanks jimmychan,

0 件の賞賛
返信