MMPF0200F6AEP for i.mx6SoloX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0200F6AEP for i.mx6SoloX

2,311件の閲覧回数
peralesserrano
Contributor I

hi

is mandatory to use MMPF0200F6AEP for i.mx6sx designs.

This IC still not sold anywhere, and I want to start my design i.mx6sx.

Is there an alternative? I do not want to program MMPF0200.

Should I use discrete components for power?

exists some reference design with components available for i.mx6sx?

ty

ラベル(1)
タグ(1)
0 件の賞賛
返信
7 返答(返信)

1,928件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi perales

it is not mandatory to use MMPF0200F6AEP,

however one needs to provide correct power-up sequence

to processor. In general one can use also discrete components for power,

however I am not aware of example schematcis for that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,928件の閲覧回数
peralesserrano
Contributor I

hi igorpadykov ty for answer.

MMPF0200F6AEP all have the same sequence on by default, but the levels of voltages are different.

secuen.png

freescale says that all support i.mx6sx, for example MMPF0200F3:

Sin nombre.png

but the levels are not the same:

f.png

can i change MMPF0200F6AEP 0 per MMPF0200F3? is posible?  Ty for answer

0 件の賞賛
返信

1,928件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

only MMPF0200F6AEP supports SX, refer to table


~igorMMPF0200.jpg

0 件の賞賛
返信

1,928件の閲覧回数
peralesserrano
Contributor I

Hi igor

This table says MMP0200F6 is used in the reference design. Others are not used. In the other reference designs MMP0100 is used.

Supported devices are on the table which I have set.

Then you can use for example MMP0200F3 or must be reprogrammed?

0 件の賞賛
返信

1,928件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi perales

This table says MMP0200F6 should be  used for any i.MX6SX

based designs.

You can program NP device also.

0 件の賞賛
返信

1,928件の閲覧回数
peralesserrano
Contributor I

hi igor sorry but I think not

This tablet says MMPF0200F6 is only used in this design (reference desing for i.mx6Sx): SABRE Board Reference Design|Freescale

MMPF0200.jpg

in other reference desing no use MMPF0200, in all use MMPF0100 so the table is empty

Sin nombre.png

SABRE Reference Designs|Freescale

dispositivos.png

sorry for my bad english

0 件の賞賛
返信

1,928件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi perales

if you are novice, it is highly recommended to use

MMPF0200F6 and i.MX6SX Sabre Board as starting

point for first design.

0 件の賞賛
返信