MMPF0200 output capacitor values

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0200 output capacitor values

1,929件の閲覧回数
vadimaleynikov
Contributor III

Hello,

Is it correct/possible to decrease the SW1A/B and SW3A/B output capacitors to 2x22uF each when the maximum loads of these regulators are limited to 1A?

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,727件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

I believe this is possible, in particular this option is mentioned in

MMPF0200 Table 70. SW3A/B External Component Requirements

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,727件の閲覧回数
vadimaleynikov
Contributor III

Hi Igor,

Thank you. Unfortunately your reference to Table 70 is applicable to SW3A/B only and I'm not sure if the SW1A/B feedback loop is stable with 2x22uF output capacitors.

Best regards,

Vadim

0 件の賞賛
返信