MMPF0100NPAEP Power-off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100NPAEP Power-off

1,646 Views
NaveenHN
Contributor II

Hi, We are using MMPF0100NPAEP for powering a general purpose SoC. PWRON is connected to VSNVS (1.8V) using a pull-up resistor and a pushbutton switch and in OTP, PWRON_CFG bit is set to 0.

When VIN power is applied and pushbutton is pressed, all the voltage rails come up as expected. When the pushbutton is pushed again or kept pressed, the device is not switching off or going to sleep mode. 

Could you please let us know what is the issue here? Am I missing anything?

Thanks,

Naveen 

Labels (2)
0 Kudos
Reply
1 Reply

1,544 Views
Yuri
NXP Employee
NXP Employee

Hello,

  From the PMIC datasheet:

The PWRON pin is used to power off the PF0100. The PWRON pin can be configured with OTP to power off the PMIC under the following [...] conditions:
1. PWRON_CFG bit = 0, SWxOMODE bit = 0 and PWRON pin is low.

...

  Any regulators whose SWxOMODE bit is set to “1” enters Sleep mode if a PWRON turn-off event occurs, and any regulator whose SWxOMODE bit is set to “0” turns off.

  Is it possible to check SWxOMODE bit?


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply