MMPF0100F0EP reprogrammability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100F0EP reprogrammability

1,581 Views
vinodkumar
Contributor I

Hi,

We are using Freescale PMIC Part number MMPF0100F0EP in our project.

It is a pre-programmed device. We are planning to reprogram again using I2C interface.

Please Let us know whether PMIC part number MMPF0100F0EP can be reprogrammed using I2C interface.

Thanks in advance,

Vinod Kumar

Labels (1)
0 Kudos
Reply
2 Replies

1,432 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Vinod Kumar,

Yes, it is totally possible to re-program the MMPF0100 devices using I2C interface, it can be “OTP (One Time Programming) programmable” or “TBB (Try Before Buy) programmable”. All the instructions about how to do this is mentioned in the application note AN4536

Just be advice that it is possible to program bits which are “0” to “1”. But if they are already pre-programmed with “1” on the fuses, they cannot be changed to “0”.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,432 Views
gusarambula
NXP TechSupport
NXP TechSupport

reyes Would you please comment on this scenario?

0 Kudos
Reply