MMPF0100 in u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MMPF0100 in u-boot

跳至解决方案
2,033 次查看
JHY
Contributor IV

Hi,

Below data on i2c in u-boot is from SABRE-SDB but I think it is not from PMIC.

=> i2c probe

Valid chip addresses: 08 48

=> i2c md 0x08 0 10

0000: 10 10 10 10 10 10 10 10 10 10 10 10 10 10 10 10    ................

How can access register in PMIC?

pastedImage_2.png

标记 (1)
0 项奖励
回复
1 解答
1,859 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JHY

had you implemented patch

I2C command in 2014.01 u-boot on sabresd

also could you try exlicitly set address and read data one by one

(without autoincrementing): i2c md 0x08 0.., i2c md 0x08 1.., i2c md 0x08 2..

Best regards

igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,860 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JHY

had you implemented patch

I2C command in 2014.01 u-boot on sabresd

also could you try exlicitly set address and read data one by one

(without autoincrementing): i2c md 0x08 0.., i2c md 0x08 1.., i2c md 0x08 2..

Best regards

igor

0 项奖励
回复