MMPF0100 PMIC - VTT Rail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 PMIC - VTT Rail

Jump to solution
2,654 Views
davidkearney
Contributor II

Hi There,

I'm planning  on using the MMPF0100 as the PMIC for a Zynq Z7020-based design. AN4991 has a useful reference design for this application, I just have once concern regarding VTT, the DDR3 active termination rail. This rail needs to Source and Sink current during DDR3 activity, and I don't see this explicitly addressed in the datasheet. It mentions that SW4 has a VTT mode which tracks V_DDR3/2, but in this PWM mode does it also successfully sink the required current? 

Many Thanks in advance,

Dave

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,201 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Dave,

Yes, regulators of the MMPF0100 have a strong sourcing capability and sinking capability in PWM mode, therefore, in VTT mode SW4 works only in the PWM mode to enable it to source or sink load current.

 

This can be found as a comment in section 4.7 of the application note AN4714.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,202 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Dave,

Yes, regulators of the MMPF0100 have a strong sourcing capability and sinking capability in PWM mode, therefore, in VTT mode SW4 works only in the PWM mode to enable it to source or sink load current.

 

This can be found as a comment in section 4.7 of the application note AN4714.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply