MMPF0100 PCB Guideline

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 PCB Guideline

3,526 Views
thanhnhatle
Contributor II

Hi

I am going to use MMPF0100F0ANES in our design which has the Package Outline Drawing Number 98ASA00589D.

http://cache.freescale.com/files/shared/doc/package_info/98ASA00589D.pdf

Do you have any PCB Guideline document recommend for this package 98ASA00589D as the following for package 98ASA00379D (page 4,5)?

Can 98ASA00589D package use the same PCB with 98ASA00379D ?

http://cache.freescale.com/files/shared/doc/package_info/98ASA00379D.pdf

I've referenced AN1902 (Assembly Guidelines for QFN (Quad Flat No-lead) and DFN (Dual Flat No-lead) Packages) but it is better if you have a guideline PCB for 98ASA00589D?

http://cache.freescale.com/files/analog/doc/app_note/AN1902.pdf?fasp=1&WT_TYPE=Application%20Notes&W...

Best Regards,

Nhat

Labels (1)
Tags (1)
0 Kudos
Reply
6 Replies

3,338 Views
igorpadykov
NXP Employee
NXP Employee

Hi Thanh

suggest to look at sect.7.2 PF0100 Layout Guidelines    MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,338 Views
thanhnhatle
Contributor II

Hi Igor

Thank you very much for your reply.

I have referenced section 7.2 Layout Guidelines as your suggest.

I am sorry that my question is not clearly.

I want to find the Land Pattern Design guideline for part MMPF0100F0ANES, which is not mention in section 7.2

In the datasheet of MMPF0100Z, section 8, suffix ES part (WF-Type package ) can refer to two package documents  98ASA00379D, 98ASA00589D.

Do you have the Land Pattern Design guideline for  98ASA00589D?

Can 98ASA00589D package use the same Land Pattern Design with 98ASA00379D?

Best Regards,

Nhat

0 Kudos
Reply

3,338 Views
igorpadykov
NXP Employee
NXP Employee

Hi Thanh

I think one can look at i.MX6_SABRE_SDP_DESIGNFILES : Design files, including hardware

schematics, Gerbers, and OrCAD files,

it uses MMPF0100

Best regards

igor

0 Kudos
Reply

3,338 Views
guslabao
Contributor III

Hi,

I would like to follow up with this PCB land pattern for Package Outline Drawing Number 98ASA00589D.

Would the land pattern used below work for the 98ASA00589D package?

http://cache.freescale.com/files/shared/doc/package_info/98ASA00379D.pdf

Thanks,

Gus

0 Kudos
Reply

3,338 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

3,338 Views
guslabao
Contributor III

HI Igor,

For Package Outline Drawing Number 98ASA00589D.

Is there a recommended land pattern?

Thanks,

Gus

0 Kudos
Reply