MMC unfindable after reboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMC unfindable after reboot

1,072 次查看
eal-fox
Contributor II

Hi all,

 

I have quite a strange issue and I am not sure if I am looking in the right direction, so I was hoping for some guidance.

I unfortunately can't share all of my code, but I am happy to provide some of it if necessary

 

When I boot from the EMMC on my custom board (very alike the iMX6ulEVK), I can boot into the kernel fine just once. However, if I reboot, U-boot cannot find any MMC cards anymore (I also have an SD-card plugged in). running gpio status in U-boot gives me nothing. This lead me to think that the devicetree of u-boot might have gotten corrupted. This I would find very strange though, as U-boot is stored on one of the hardware boot partitions of my EMMC and this partition is read only. (EMMC is the Kingston EMMC04G-MK27-C01C). Any help to point me in the right direction would be greatly appreciated

 

with kind regards,

Timon Vos

标记 (1)
0 项奖励
回复
1 回复

1,049 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @eal-fox 

I hope you are doing very well.

 

This is a strange issue...
Are you able to share your U-Boot and Linux DTS?

 

Also, is it possible to analyze the behavior of the related GPIOs and power lines for MMC interfaces while reboot?

 

Best regards,

Salas.

0 项奖励
回复