MMA8451Q Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMA8451Q Linux

3,072件の閲覧回数
deepanrajanbara
Contributor IV

Hi ,

We are currently using MMA8451Q 3-axis, 14-bit/8-bit digital accelerometer But we are not able to find the Linux driver for this Module.Please provide a solution on where to get the Linux driver for MMA8451Q.

Thank you,

Deepanraj.A

ラベル(3)
0 件の賞賛
返信
5 返答(返信)

2,682件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
0 件の賞賛
返信

2,682件の閲覧回数
deepanrajanbara
Contributor IV

Thank you

0 件の賞賛
返信

2,682件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Deepanraj,

IMX6 family Linux image provides generic I2C kernel drivers, but there is no specific application driver for this sensor in Linux, this must be developed by the user.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,682件の閲覧回数
deepanrajanbara
Contributor IV

Can i get generic I2C kernel drivers for MMA8451Q.

Thank you,

Deepanraj.A

0 件の賞賛
返信

2,682件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Unfortunately there are no Linux drivers for this device. In the following document you can find a baremetal driver which you can use as a base to develop your own driver.

https://community.nxp.com/docs/DOC-98836 

Regards,

Carlos

0 件の賞賛
返信