MK22FN512VLH12,MK22FN128VLH10 Temperature Range Modify!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK22FN512VLH12,MK22FN128VLH10 Temperature Range Modify!

1,189 Views
Leaderdavid88
Contributor I

Hi Greg, 

The MK22 parts as below which Operating Characteristics • Voltage range (including flash writes): 1.71 to 3.6 V • Temperature range (ambient): -40 to 105°C. The client doesn’t need -40°C and the exact temperature range is needed 0°C to 70°C. When we was modified temperature then we estimated the order quantities 10M pieces.

In fact, we have ordered below samples, but the lead time in 2023, it is too late, would you please support us to change temperature then we can avoid to meet MK22 shortage of problem.

Right now, could you support us these items one piece/per item sample in May 2022 before. We will place order each 500K/yr in 2022.

  1. NXP:MK22FN512VLH12:
  2. NXP:MK22FN128VLH10:

On the other hand, please support us below parts for sample test, we estimated the exact quantities are 10M pieces.

  1. NXP: MK22FN512VLH12: 1.6K sample 
  2. NXP: MK22FN128VLH10: 1.6K sample
  3. NXP: LPC1837JBD144E:   2tray sample

We'll look forward your reply. Thanks.

Best Regards

David Liu

[email protected]

 

0 Kudos
Reply
2 Replies

1,147 Views
Leaderdavid88
Contributor I

Hi Greg, 

The MK22 parts as below which Operating Characteristics • Voltage range (including flash writes): 1.71 to 3.6 V • Temperature range (ambient): -40 to 105°C. The client doesn’t need -40°C and the exact temperature range is needed 0°C to 70°C. We plan order $ 50 US. May we support you to contact with foundry to produce it ASAP. Tks.

0 Kudos
Reply

1,145 Views
Leaderdavid88
Contributor I
The MK22 parts as below which Operating Characteristics • Voltage range (including flash writes): 1.71 to 3.6 V • Temperature range (ambient): -40 to 105°C. The client doesn’t need -40°C and the exact temperature range is needed 0°C to 70°C. We plan order $ 50M US. May we support you to contact with foundry to produce it ASAP. Tks.

0 Kudos
Reply