MK22FN512VLH12,MK22FN128VLH10 Temperature Range Modify!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK22FN512VLH12,MK22FN128VLH10 Temperature Range Modify!

1,139 次查看
Leaderdavid88
Contributor I

Hi Greg, 

The MK22 parts as below which Operating Characteristics • Voltage range (including flash writes): 1.71 to 3.6 V • Temperature range (ambient): -40 to 105°C. The client doesn’t need -40°C and the exact temperature range is needed 0°C to 70°C. When we was modified temperature then we estimated the order quantities 10M pieces.

In fact, we have ordered below samples, but the lead time in 2023, it is too late, would you please support us to change temperature then we can avoid to meet MK22 shortage of problem.

Right now, could you support us these items one piece/per item sample in May 2022 before. We will place order each 500K/yr in 2022.

  1. NXP:MK22FN512VLH12:
  2. NXP:MK22FN128VLH10:

On the other hand, please support us below parts for sample test, we estimated the exact quantities are 10M pieces.

  1. NXP: MK22FN512VLH12: 1.6K sample 
  2. NXP: MK22FN128VLH10: 1.6K sample
  3. NXP: LPC1837JBD144E:   2tray sample

We'll look forward your reply. Thanks.

Best Regards

David Liu

[email protected]

 

0 项奖励
回复
2 回复数

1,097 次查看
Leaderdavid88
Contributor I

Hi Greg, 

The MK22 parts as below which Operating Characteristics • Voltage range (including flash writes): 1.71 to 3.6 V • Temperature range (ambient): -40 to 105°C. The client doesn’t need -40°C and the exact temperature range is needed 0°C to 70°C. We plan order $ 50 US. May we support you to contact with foundry to produce it ASAP. Tks.

0 项奖励
回复

1,095 次查看
Leaderdavid88
Contributor I
The MK22 parts as below which Operating Characteristics • Voltage range (including flash writes): 1.71 to 3.6 V • Temperature range (ambient): -40 to 105°C. The client doesn’t need -40°C and the exact temperature range is needed 0°C to 70°C. We plan order $ 50M US. May we support you to contact with foundry to produce it ASAP. Tks.

0 项奖励
回复