MIPI camera for SABRE AI EVK.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI camera for SABRE AI EVK.

1,790 Views
shyamjithkv
Contributor III

Hi,

I'm using imx SABRE AI EVK board from freescale, I'm in need of a MIPI camera that can be connected to J7 MIPI connector (60 pin) of MCIMX6AICPU2.Please provide information on where i can buy a compatible one.

Thanks in advance.

Labels (4)
0 Kudos
Reply
2 Replies

1,572 Views
igorpadykov
NXP Employee
NXP Employee

Hi shyamjith

please look at

Re: camera

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,572 Views
shyamjithkv
Contributor III

Thank you igorpadykov​

I'm looking for a plug-in camera module which can be plugged in straight away to 60 pin MIPI connector on imx6 CPU board.

Do you know any of that kind?

Best Regards

0 Kudos
Reply