MIPI Gasket, IPU, CSI and Device tree

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI Gasket, IPU, CSI and Device tree

ソリューションへジャンプ
3,581件の閲覧回数
davider
Contributor II

Hello,

  I'm trying to write a DTS (Linux 3.10.17) for our custom designed board. I need to use all the 4 i.MX6D/Q CSI interfaces to acquire 4 MIPI streams on 4 virtual channels simultaneously.

  Is it possible using existent drivers and bindings, or does it require to extend their functionalities (or to write a new driver)?

ラベル(2)
タグ(5)
0 件の賞賛
返信
1 解決策
2,563件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Davide

yes this will require new drivers, also it may be useful

to check below discussion. Existent drivers and bindings

support only i.MX6 Sabre reference board configuration (one MIPI and one CSI parallel camera)

4 video capture using MIPI-CSI2 port

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,564件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Davide

yes this will require new drivers, also it may be useful

to check below discussion. Existent drivers and bindings

support only i.MX6 Sabre reference board configuration (one MIPI and one CSI parallel camera)

4 video capture using MIPI-CSI2 port

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,563件の閲覧回数
davider
Contributor II

Ok, thank you.

You have confimed my fears... Even if it does not seems that difficult to extend the whole stuff, it will nonetheless be quite time consuming.

0 件の賞賛
返信