MIPI DSI support for i.MX 8QuadXPlus in Android P9.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI DSI support for i.MX 8QuadXPlus in Android P9.0.0

ソリューションへジャンプ
1,339件の閲覧回数
pierluigi_p
Contributor V

Hi,

specifically referring to iMX8QXP, in Android 9 NXP provides a single dtbo, only supporting HDMI using LVDS to HDMI bridge.

I'm not able to find references to MIPI DSI support, neither in the boot options nor in the documentation.

Is MIPI DSI interface actually supported in Android for iMX8QXP?

Thanks

Best Regards

Pier

ラベル(1)
1 解決策
1,071件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Please take a look to the table 5.2 Board images of the Android_Quick_Start_Guide.pdf, that I'll attach here, there you'll note that the single dtbo will have it added:
 dtbo-imx8qxp.img

 - dtbo_a and dtbo_b partitions to support single LVDS-toHDMI/MIPI-to-HDMI or dual LVDS-to-HDMI displays with dual-camera support.

 

Also, please remember that the i.MX8X is still under pre-production stage so our support is limited, thank you.

 

Hope this helps,

Best regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,072件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Please take a look to the table 5.2 Board images of the Android_Quick_Start_Guide.pdf, that I'll attach here, there you'll note that the single dtbo will have it added:
 dtbo-imx8qxp.img

 - dtbo_a and dtbo_b partitions to support single LVDS-toHDMI/MIPI-to-HDMI or dual LVDS-to-HDMI displays with dual-camera support.

 

Also, please remember that the i.MX8X is still under pre-production stage so our support is limited, thank you.

 

Hope this helps,

Best regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信