MIPI DSI mipi clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI DSI mipi clock

3,474 Views
felixh
Contributor I

Hi

I'm using  a Agilent DSO9084A Oscilloscope to analyze a two lane MIPI DSI bus.

The MIPI analyzation software don't use the external MIPI clk  from the imx6 cpu, but instead needs the data rate specified.

I need to know the exact mipi clk used when configuring my display.

For example, when i configure my display to use a max_phy_clk=300, in mipi_lcd_config,  what is the exact mipi clk generated from this.

I'm using kernel driver from branch imx_3.14.38_6qp_ga

Best Regards

Felix

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

2,130 Views
b36401
NXP Employee
NXP Employee

MIPI DSI interface of i.MX6S processor supports from 80 Mbps up to 1 Gbps speed per data lane.

DSI receiver cores can mange one clock lane and up to 4 data lanes through the lane management,

however two data lanes are implemented in the transmitter D-PHY, therefore the maximum throughput of display port is 2Gbps.

Please refer to 9.10.2 and 9.10.3 chapters of i.MX 6Solo/6DualLite Applications Processor Reference Manual for more details.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply