MIPI Camera capture on ubuntu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI Camera capture on ubuntu

3,483件の閲覧回数
ahmedtolba
Contributor I

Hi All,

I would like to ask if its possible to use/ capture the data from the mipi-csi2 port on ubuntu using your current driver and mx6?

I would like to just capture it  without v4l2, just want to capture pure packets then use SDL or any OpenGL to render the data

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,465件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I would start trying unit_test capture test.

Do you have the folder /unit_test?

find for some test with capture within the name.

Then you can try to capture something using your camera. What camera are you using?

0 件の賞賛
返信

2,465件の閲覧回数
ahmedtolba
Contributor I

I don't have a unit test.

I'm using  Samsung 5Mpixel K5ECG MIPI CSI sensor

0 件の賞賛
返信

2,465件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

So, find the unit_test and use ti.

I think you would need to install it. (sorry, I´m not used with Ubuntu rootfs)