Dear NXP Support,
please describe the IMX8MP MIPI_CSIx_DPHY_COMMON_CTRL register HSSETTLE field:
There are multiple sources with tables relating to a number to frequency, eg:
https://community.nxp.com/t5/i-MX-Processors/raw12-camera-on-imx8mp-isi/m-p/1663012/highlight/true#M...
But I would like a formal description, since the values that I am experimenting with do not fit the table of other posts. My MIPI CSI Phy runs at 300Mhz/600Mbps, and a csis-hs-settle = <6> is generating a lot of SOT errors. When I use csis-hs-settle = <13> there are no errors.
Thank you for your support.
Best regards,
Ian
解決済! 解決策の投稿を見る。
Hi @Eximius
The suggested setting in that table will make the Ths-settle in the middle of the range (about 95ns to 156.67ns for 600Mbps).
Hi @Eximius
The left column of the table is Mbps, date rate, it is not MIPI clock frequency, so your data rate is 600Mbps, value 13 is the correct one.
Hi @Eximius
The suggested setting in that table will make the Ths-settle in the middle of the range (about 95ns to 156.67ns for 600Mbps).
sent to you via mail, pls check